MC3390X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC3390X

1,001 Views
mauriziogreco
Contributor III

Hi, we are working with MC3390X.

Can someone help us to find a way to communicate with this device in order to init the windowed watchdog and in some conditions ask to device to disable the watchdog (for example in order to flashing some areas) ?

Thanks in advance.

2 Replies

801 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

which MC3390x do you exactly have?

Is it can transceiver, SBC chip or what?

pastedImage_1.png

Peter

801 Views
mauriziogreco
Contributor III

Hi, thanks very much for your support.

The device is MC33907-MC33908D2.

Today I'm working on disable and re-enable the windowed watchdog. Now it

seems it works.

My current approach is:

- starting with WD enabled (i.e. 128ms) into BootLoader, before jump into

applicative code, disable the WD (i.e setting 0 ) .

- when the Program Counter will be into Applicative Code no performing

init of device MC33907-MC33908D2.

- performing the enable of WD (setting i.e 128ms)

When I must reflash code applicative:

- disable the WD and after jump into bootloader (in order to flashing code)

asking a RESET of uP

- in Boot Code, keep WD enabled (i.e. 128ms) but before erase flash of

applicative code, disable the WD (i.e setting 0 ) .

- erasing and programming flash from Bootloader

- return in applicative layer (exit from BOOT) and no execute re-init of

the MC33907-MC33908D2.

- enable the WD

With this "approach", now it is working fine for me.

2017-04-19 8:02 GMT+02:00 petervlna <admin@community.nxp.com>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: MC3390X

reply from Peter Vlna

<https://community.nxp.com/people/petervlna?et=watches.email.thread> in

MPC5xxx - View the full discussion

<https://community.nxp.com/message/897974?commentID=897974&et=watches.email.thread#comment-897974>

0 Kudos
Reply