LIN code for mpc 5777c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LIN code for mpc 5777c

1,225 Views
qudgus877
Contributor I

Hi, I studying LIN communication for mpc 5777c. I'm looking for LIN example code for mpc 5777c but I can't found it. Can I get some help for this code? I want to transmit and recieve multiple data but it doesn't work. Here's the code. 

#define esci_c
#include "..\typedefs_mpc.h"
#include "..\proto_mpc.h"
 
void esci_init(void)
{
LIN_EN = 1;
SIU.PCR[LIN_TXD_pin].R = 0x400; // Configure pad for primary func: LIN_TXD
SIU.PCR[LIN_RXD_pin].R = 0x400; // Configure pad for primary func: LIN_RXD
 
eSCI_B.CR2.R = 0x2000; // module is enabled (default setting)
eSCI_B.LCR1.R = 0x0000;  // LIN module deactivation
 
eSCI_B.BRR.B.SBR = 625;
 
eSCI_B.LCR1.B.LIN = 1;  // LIN module activation
        eSCI_B.CR2.B.BRCL = 1;
        eSCI_B.CR2.B.BESTP = 1;
        eSCI_B.CR2.B.BSTP = 1;
eSCI_B.CR1.B.TE = 1; // Tx enabled
eSCI_B.CR1.B.RE = 1; // Rx enabled
 
// transmit interrupt activation
eSCI_B.CR1.B.RIE = 1;
}
 
uint8_t lin_data = 0x2;
uint8_t receivedID;
 
// frame transmit
void LIN_SendFrame(uint8_t header, uint8_t* data, uint8_t length)
{
   //eSCI_B.LRR.R = header;
 
   uint8_t j = 0; /* Dummy variable */
   for (j=0; j<length; j++)
   {
      if(eSCI_B.IFSR2.B.TXRDY == 1)
      {
         eSCI_B.IFSR2.R = 0x4000; /* Clear TXRDY flag */
         eSCI_B.LTR.R = *(data+j); /* Transmit 8 bits Data */
      }
   }
}
 
#define MY_ID 0x15
uint8_t test_lin = 0;
// frame receive
void LIN_ReceiveFrame(uint8_t* header, uint8_t* data, uint8_t length)
{
 
   uint8_t j = 0; /* Dummy variable */
 
   if (eSCI_B.IFSR2.B.RXRDY == 1)
   {
      eSCI_B.IFSR2.B.RXRDY = 0x8000; /* Clear RXRDY flag */
      *header = eSCI_B.LRR.R;
      if (*header == MY_ID)
      {
         test_lin = 1;
         for (j=0; j<length; j++)
         {
            eSCI_B.IFSR2.B.RXRDY = 0x8000; /* Clear RXRDY flag */
            *(data + j) = eSCI_B.LRR.R; /* Read byte of Data*/
         }
      }
   }
}
 
void LIN_IRQHandler(void) {
 
 
    if (eSCI_B.IFSR2.B.OVFL) 
    {
    eSCI_B.IFSR2.B.OVFL = 0;
    }
 
    if (eSCI_B.IFSR2.B.RXRDY) 
    {
        uint8_t receivedID = eSCI_B.LRR.R;
 
        if (receivedID == MY_ID) 
        {
        uint8_t receivedData = eSCI_B.LRR.R;
        }
        eSCI_B.IFSR2.B.RXRDY = 0;
    }
 
    if (eSCI_B.IFSR2.B.TXRDY) 
    {
    eSCI_B.IFSR2.B.TXRDY = 0;
    }
}
 
 
   uint8_t txHeader = 0x01;
   uint8_t txData[] = {0x15, 0x22, 0x33,0x44};
   LIN_SendFrame(txHeader, txData, 4);
   LIN_ReceiveFrame(&rxHeader, rxData, 4);

 

Tags (1)
0 Kudos
Reply
1 Reply

1,174 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can refer to code posted at https://community.nxp.com/t5/MPC5xxx/LIN-implementation/td-p/1190510

BR, Petr

0 Kudos
Reply