Is there a pin wizard tool and code generation tool for the MPC5744P?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a pin wizard tool and code generation tool for the MPC5744P?

1,958 Views
terryk
Contributor I

Hi,

Is there a pin wizard tool and code generation tool for the MPC5744P such as [Processor Expert, RAppID Suite Pin Wizard for MPC5746M] ?

I have a GHS compiler and an S32_Power_v1.1 compiler. And it is not OS and Autosar development environment.

0 Kudos
Reply
3 Replies

1,804 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

you can use RAppID Initialization for Power Architecture. Please check the link below.

RAppID Initialization for Power Architecture|NXP 

Regards,

Martin

0 Kudos
Reply

1,804 Views
terryk
Contributor I

Hi,

I checked that link. 

However, I could not find information of [mpc5744p] in the [archived] category or [Initialization / Boot / Device Driver Code Generation].

I tried importing and running [Processor Expert RAppID Suite Pin Wizard for MPC5748G (REV 1.0.1)] in the [RAppID Suite v10.2.1] tool, but [MPC5748G]  It looks a lot different from [MPC5744P].

How can I use the [RAPPID: RAppID Initialization for Power Architecture] tool as a pin wizard and code generator for [MPC5744p]?

0 Kudos
Reply

1,804 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I am very sorry for my previous answer, RAppID Initialization for Power Architecture does not support MPC5744P. Unfortunately, there is no another tools which could be used for MPC5744P (pin) initialization.

Regards,

Martin

0 Kudos
Reply