IVOR 1 while initializing HSM in MPC5748G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IVOR 1 while initializing HSM in MPC5748G

1,884件の閲覧回数
tejo2one
Contributor III

I have a working code where I want to integrate HSM.

After calling HSM_DRV_Init, during SetInterrupt mcu is entering IVOR1 error ?

What could be causing this? and how to resolve it?

tejo2one_0-1680799244296.pngtejo2one_0-1680799244296.png

tejo2one_0-1680801496141.pngtejo2one_0-1680801496141.png

 

0 件の賞賛
返信
3 返答(返信)

1,851件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

and do you have NXP HSM FW programmed in device or custom one?

If yes, which version?

Best regards,

Peter

0 件の賞賛
返信

1,836件の閲覧回数
tejo2one
Contributor III

Hello Peter,

I'm working using Devkit of MPC5748G. Is there a separate process to get HSM firmware ?

please provide more information, thank you.

Best regards,

Tejo

0 件の賞賛
返信

1,832件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

To get HSM FW the part must come from NXP factory with already preprogramed HSM FW.

Such part is not commonly available and need to be asked via sales / distributor.

So in order to use HSM you either has NXP or third party FW or you are going to develop it yourself, which will require access to very sensitive documentation.

Parts with HSM FW starts with KC6676x instead of SPC57xx.

Best regards,

Peter

0 件の賞賛
返信