I2C interface with MPC5200

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C interface with MPC5200

2,110 Views
ashwinibhat
Contributor II

Please provide flow to work I2C interface on MPC5200

Labels (1)
3 Replies

2,001 Views
Pavel
NXP Employee
NXP Employee

Look at attached file. It is simple I2C program example for the MPC5200B board. It is CodeWarrior project for the Lite5200B board.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,001 Views
ashwinibhat
Contributor II

Thanks Pavel.

I will refer this source code.

0 Kudos
Reply

2,000 Views
ashwinibhat
Contributor II

Can anybody tell answer of this question?

0 Kudos
Reply