I learned from the manual before doing FFT processing ADC format can be tile4 or tile8, the two formats are just arranged differently? Which one is more suitable for processing, processing faster?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I learned from the manual before doing FFT processing ADC format can be tile4 or tile8, the two formats are just arranged differently? Which one is more suitable for processing, processing faster?

1,456 次查看
yinlei
Contributor III

I learned from the manual before doing FFT processing ADC format can be tile4 or tile8, the two formats are just arranged differently? Which one is more suitable for processing, processing faster?

标记 (3)
0 项奖励
回复
1 回复

1,348 次查看
taokang
Contributor III

hello,

The tile 8 is best suitable for FFT processing.Because the TRAM/ORAM is accessed 8 slice at once.