I learned from the manual before doing FFT processing ADC format can be tile4 or tile8, the two formats are just arranged differently? Which one is more suitable for processing, processing faster?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I learned from the manual before doing FFT processing ADC format can be tile4 or tile8, the two formats are just arranged differently? Which one is more suitable for processing, processing faster?

1,472件の閲覧回数
yinlei
Contributor III

I learned from the manual before doing FFT processing ADC format can be tile4 or tile8, the two formats are just arranged differently? Which one is more suitable for processing, processing faster?

タグ(3)
0 件の賞賛
返信
1 返信

1,364件の閲覧回数
taokang
Contributor III

hello,

The tile 8 is best suitable for FFT processing.Because the TRAM/ORAM is accessed 8 slice at once.