How to use MPC5777M ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use MPC5777M ?

1,875 Views
dukaizhu
Contributor I

1.  MPC5777M have six LINFlexD modules in the reference manual of MPC5777M, but it does not describe that which three  LINFlexD modules can be configurable as LINFlexD mode, and which three  LINFlexD modules can be configurable as UART mode.

2.  How many external interrupt request pin does MPC5777M have ?  It sometimes describe 9 or 8  ? 

3.  MPC5777M have three reset pin, they are  PORST, ESR0 and ESR1, how to use them  ?

    How  these three reset pin be connected to  35FS6500 SBC ?

     

0 Kudos
Reply
1 Reply

1,788 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi,

1) Each LINFlexD is capable to run in both LIN and UART mode.

2) Neither 8 nor 9. Correct number is 10.

pastedImage_2.png

3) PORST assertion causes destructive reset, ERS0 functional reset and ERS0 is configurable for NMI, safe mode or functional reset.

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

0 Kudos
Reply