How to start emulation debug on MPC5777C with PE Micro debugger ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to start emulation debug on MPC5777C with PE Micro debugger ?

2,289件の閲覧回数
trevorlin
Contributor I

I have try to programming MPC5777C with ICE .
but it's alwasy feedback "can't enter BDM mode"
I have check 1.25V on VDD pin, 8MHz clock on EXTAL, 3.3V on VDDEx, VDDPMC, VDDPWR
and all of JTAG I/F connection is correct .
Is anybody give some suggest ?

0 件の賞賛
返信
2 返答(返信)

2,149件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

which IDE you use?

What is the microcontroller mask?

Regards,

Martin

0 件の賞賛
返信

2,149件の閲覧回数
trevorlin
Contributor I

dear Marin

Our platform choose SPC5777CK3MME3 as second core .

, and I choose S32 design studio as IDE .

I have try to connect to device , but it's halt on enter Debug session . 

未命名 (132).png未命名 (131).png

I assumed this problem may be caused by some kind of setting .

But I can't solved it.

please give me some suggest for debug .

0 件の賞賛
返信