I have downloaded the the AUTOSAR 4.0.92 RTM 10.3 and was able to build the sample application sc2 using green hills compiler and load it onto MPC5748G LCEVB and run it and confirmed that LED1 is on.
Now, how do I import the oil or epc into the EB tresos 14.2.1?
I tried the following:
For oil file, I tried:
C:\EB\tresos\bin\tresos_cmd_64.bat -Dtarget=5748G -Doil.include=C:\Autosar\sc2\src -Doil-package=Os -Doil.config=Os legacy convert sample2.oil output.epc
And it printed:
EB tresos Studio 14.2.1 b140128-1223
Copyright 2003-2014 Elektrobit Automotive GmbH
Licensed to: Freescale
ERROR 21-07-30,13:47:50 (2118) The content type oil is unknown. Cannot process files.
Errors "1" Warnings "0"
For epc file, I created a new Configuration Project with AUTOSAR version of 4.0.3. with ECU id of MPC5748G, and selected the target of PA/MPC574XG and left everything else as default.
In the Module Configuration, I hit next (so only Resource was selected). I pressed "+" icon in the importers/exports page and called it epc and pressed next. For Autosar options:
Filename: sample2_5748G.epc
Content type: asc:4.0.3
Import strategy: Replace.
And pressed Finished. And Finished on the main new project wizard.
It did the importer processing and I got:
Warning: (20011) Nothing to import in file sample2_5748G.epc.
Any help would be appreciated.
Thanks, Danny