How do I know what the interrupt source is?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I know what the interrupt source is?

ソリューションへジャンプ
1,671件の閲覧回数
CoinFish
Contributor I

I‘m using mpc5675k device, I often trigger interrupts inexplicably when debugging.

I know that because I did not configure the corresponding interrupt, the program often runs into the DefaultInterrupt function.

What confuses me is that I know I have not configured it, but I don't know what the interrupt source is. This often takes me a lot of time. Is there any way to quickly know what the interrupt is?

 

/**
 * This is the default interrupt service routine for non-implemented
 * exceptions and interrupts.
 */
void DefaultInterrupt(void)
{

    while(1)
    {
        /* Freeze, the non-implemented exceptions and interrupts fires?
         * TODO: It is users responsiblity to consider and implement proper actions on what to do
         *       to response which non-implemneted/unexpected interrupts.
         */
         if(STD_ON == RGM_AlternateModeOccured())
         {
             break;
         }
    }
}
0 件の賞賛
返信
1 解決策
1,664件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

You haven't stated used compiler or mode (HW/SW) or whehter you mean interrupt or exception. Anyway considering CodeWarrior 2.10, used startupt code contain INTC_INTCInterruptHandler function, where you can put breakpoint and analyze ISR code flow. For exceptions there ivor_branch_table_p0, usually ending in IVOR traps.

General description of interrupts:

It is quite well described in following appnote:

http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf

 

Figure 9 describes SW vector more, Figure 12 describes HW vector mode.

 

Most of the customer use SW vector mode. It is like “default” mode. HW vector mode you would use in case you would need extremely fast ISR response for some sources - the disadvantage would be this approach takes more memory. If you currently don’t have specific requirements, use software vector mode.

 

First let me clarify terminology regarding exceptions and interrupts:

Considering SW mode, all sources routed from interrupt controller into IVOR4 can be told as “interrupt” (RM names it as external interrupt), all other IVORs may be considered as “exception” (RM says interrupt). Little bit confusing but common terminology from outside world is exception and interrupt.

 

Some notes to HW vector mode - As AN2865 explains it well I would only added some info how to deal with exceptions and interrupts handlers in one project.

 

Exception branch table must be located above or behind interrupt branch table in dependency on used core as follows:

e200z1, z3, z4, z6, z7:

ISR address = IVPR + offset given by INTVEC

ESR address = IVPR + offset given by particular IVOR register (IVOR4 inactive)

Thus it means you must set IVORx register to have final address behind interrupt branch table.

 

e200z0 (all offset are fixed):

ESR address = IVPR + fixed offset starting from 0x0000

ISR address = IVPR + fixed offset starting from 0x0800

Thus in this case exception table is before interrupt table.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,665件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

You haven't stated used compiler or mode (HW/SW) or whehter you mean interrupt or exception. Anyway considering CodeWarrior 2.10, used startupt code contain INTC_INTCInterruptHandler function, where you can put breakpoint and analyze ISR code flow. For exceptions there ivor_branch_table_p0, usually ending in IVOR traps.

General description of interrupts:

It is quite well described in following appnote:

http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf

 

Figure 9 describes SW vector more, Figure 12 describes HW vector mode.

 

Most of the customer use SW vector mode. It is like “default” mode. HW vector mode you would use in case you would need extremely fast ISR response for some sources - the disadvantage would be this approach takes more memory. If you currently don’t have specific requirements, use software vector mode.

 

First let me clarify terminology regarding exceptions and interrupts:

Considering SW mode, all sources routed from interrupt controller into IVOR4 can be told as “interrupt” (RM names it as external interrupt), all other IVORs may be considered as “exception” (RM says interrupt). Little bit confusing but common terminology from outside world is exception and interrupt.

 

Some notes to HW vector mode - As AN2865 explains it well I would only added some info how to deal with exceptions and interrupts handlers in one project.

 

Exception branch table must be located above or behind interrupt branch table in dependency on used core as follows:

e200z1, z3, z4, z6, z7:

ISR address = IVPR + offset given by INTVEC

ESR address = IVPR + offset given by particular IVOR register (IVOR4 inactive)

Thus it means you must set IVORx register to have final address behind interrupt branch table.

 

e200z0 (all offset are fixed):

ESR address = IVPR + fixed offset starting from 0x0000

ISR address = IVPR + fixed offset starting from 0x0800

Thus in this case exception table is before interrupt table.

0 件の賞賛
返信