This was handled and solved through Support Request.
The kit is preloaded with the application SW so can work standalone, but there could be issues with FreeMASTER control.
Thus it is recommended to do below steps...
- the development kit is updated with the downloaded application software. User will need to compile the application in S32DS as the package does not include output elf files.
- in FreeMASTER project Options user should select correct COM number for assigned virtual serial port as per PC device manager. Finally point properly to project's MAP/elf file in "MAP Files" tab.
BR, Petr