Generating MCAL3.0 mpc563xM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generating MCAL3.0 mpc563xM

5,743 Views
Ehsaaan
Contributor III

Hello Dears.

I am using EB Tresos V27.1.0 to integrate MCAL3.0 for mpc574xM. I downloaded this MCAL package from NXP.com (MPC563XM_MCAL3.0_RTM_2.0.0_signed). 

When importing this example into the EB Tresos and generate the project, it has some errors. the screenshots of errors are attached here.

By the way, this MCAL version had some Hotfixes files, for the Resource module and ADC module that I replace the old modules with them. but still, errors are remaining.

What's wrong?

 

0 Kudos
Reply
4 Replies

5,733 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @Ehsaaan 

As the release note, this MCAL package has been tested with "Tresos 2010a.sr4 20100415-release2010a-sr4" but not tresos 27.

Could you please use the "Tresos 2010a.sr4 20100415-release2010a-sr4".

 

Module configurations were developed and tested using Tresos Configuration Tool Tresos 2010a.sr4
20100415-release2010a-sr4

Best regards,

Hung

0 Kudos
Reply

5,725 Views
Ehsaaan
Contributor III

Ok, thanks.

But where and how can I download this version("Tresos 2010a.sr4 20100415-release2010a-sr4") ?
Is it available on NXP.com with its evaluation license?

0 Kudos
Reply

5,718 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @Ehsaaan ,

 

Please access the link https://www.nxp.com/webapp/swlicensing/swlicensingIntermediate.sp

hungnguyenphi_0-1623305587083.png

 

hungnguyenphi_1-1623305638720.pnghungnguyenphi_2-1623305693371.png

hungnguyenphi_3-1623305744766.png

 

Best regards,

Hung

0 Kudos
Reply

5,714 Views
Ehsaaan
Contributor III

Tnx a lot.
Let me check.

0 Kudos
Reply