For MPC5634M MCAL ArMajorVersion: Invalid value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For MPC5634M MCAL ArMajorVersion: Invalid value

2,495件の閲覧回数
Vasily_Wu
Contributor III

When I using MPC5634M MCAL in EB Tresos, the default value of  ArMajorVersion is 0, I can not change it to 3.

Invalid value for node "/AUTOSAR/TOP-LEVEL-PACKAGES/Resource/ELEMENTS/Resource/CommonPublishedInformation/ArMajorVersion": Value out of range: is "0" but must be ">= 3" and "<= 3"

 

0 件の賞賛
返信
1 返信

2,486件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello @Vasily_Wu,

The MPC563xM MCAL 3.0 is verified with Tresos 2010a.sr4. So you should download it to use along with the MPC563xM package. As I have checked, the package works fine with Tresos 2010a

namnguyenviet_0-1631604270813.png

Best Regards,

Nam

 

0 件の賞賛
返信