For LIN protocol on MPC5748, how to we get the header ID to communicate with slave in loop back mode.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For LIN protocol on MPC5748, how to we get the header ID to communicate with slave in loop back mode.

2,083件の閲覧回数
anishchoudhary
Contributor III

I am test loop back on that code, that present in S32 Design Stdio software.

タグ(1)
6 返答(返信)

1,767件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Slave is not able to generate the header itself, so testing in the loopback make no sense, I think.

BR, Petr

1,767件の閲覧回数
anishchoudhary
Contributor III

Hi Petr,

I am just want to understand the working of LIN protocol so try to test loop back, in that i am transmitting the header by master and just see the data transmission flag is set or not but it is not set.In transmission and receiving side I am taking same ID.

Thank you for helping.

0 件の賞賛
返信

1,767件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you are using the MPC5748G EVB, then note the LIN transceiver is not powered from the EVB, thus the transmission will not work, because of bit error (RX pin does not see the same signal that is on TX pin).

So connect 12V to the LIN connector (P11.3 or P9.3)) to power the transceiver. This enables the LIN transceiver to loop TX back to RX so entire transmit frames can be issued successfully.

BR, Petr

1,767件の閲覧回数
anishchoudhary
Contributor III

Hi,

In loop back mode i am able to transmit the data and Data Transfer Flag is set, but in receiver side before Data Reviver Flag is getting set LIN bus reached in idle state because of OCF bit of LINESR register. Please help me out to resolve that.

0 件の賞賛
返信

1,767件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

try to clear LINTCSR[IOT] bit, so LIN state machine does not reset to Idle on timeout.

BR, Petr

1,767件の閲覧回数
anishchoudhary
Contributor III

Hi Petr,

How to change the baud rate for LIN protocol.

0 件の賞賛
返信