FlexRay WakeUp Channel B not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexRay WakeUp Channel B not working

1,452 Views
Macware
Contributor I

Im using MPC5478G

Flexray channel used: Channel B

The flexray status stays in UNDEFINED and no there is no communication when wakeup is enabled in channel B. The is no issue when wake up is disabled

Macware_0-1692701693794.png

The issue seems to be only in channel B, it works fine when using Channel A

Tags (1)
0 Kudos
Reply
2 Replies

1,426 Views
Macware
Contributor I

Thanks for the update. It works now

0 Kudos
Reply

1,435 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Are you using single channel mode?

davidtosenovjan_0-1692710739803.png

 

0 Kudos
Reply