FlexCAN CRC failure handling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexCAN CRC failure handling

2,206 Views
subash_sundares
Contributor I

We are using MPC5554 controller and CAN (FlexCAN2) is being used for communication between processors. The question is if the CRC failure is identified in CAN hardware, will the message buffer data is discarded or only status flag (CANx_ESR->CRCERR) is set.

Tags (2)
2 Replies

2,125 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

only a message without any CAN protocol error detected is stored into Message buffer, so yes received message in RX SMB is discarded.

BR, Petr

2,126 Views
subash_sundares
Contributor I

Thank you so much BR, Petr.

0 Kudos
Reply