FCCU-MEMU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FCCU-MEMU

1,813 Views
abdelrhman
Contributor III

for MPC5744p, I successfully injected a one bit correctable error in DMA, and that reflected to MEMU module setting the error bit flag in error flag register (MEMU_ERR_FLAG). however, this error didn't reach the FCCU module NCF_Sn registers. moreover, setting some bits in the debug register, to check the connection between the FCCU and the MEMU modules, does not set the corresponding bits in FCCU as well ?

what is the reason ??

0 Kudos
Reply
1 Reply

1,805 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am not entirely sure if I understand the steps you take correctly from your explanation.

But in case you inject the Peripheral RAM ECC correctable error, and it is reflected in MEMU, then all you need to do is to set up reporting to FCCU from MEMU.

petervlna_0-1646740408139.png

Once setup, you will see NCFS0[18] flag set in FCCU when you perform FCCU read procedure. (not visible if you do not change OP to 0xA in FCCU CFG)

For fault reads refer to:

https://www.nxp.com/docs/en/application-note/AN5284.pdf

Best regards,

Peter

 

0 Kudos
Reply