Error with my first FREERTOS Projekt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error with my first FREERTOS Projekt

1,409 次查看
Elsa_24
Contributor II

Hi,
I try to create my first project with FREERTOS. But once the project is created and I add the FREERTOS Module and generate, as soon as I do the Build I get this error:

"Description Resource Path Location Type
fatal error: FreeRTOSConfig.h: No such file or directory portasm.s "

while the file FreeRTOSConfig.h is already present in the generated File..

How to correct it please

Thank you

 

0 项奖励
回复
1 回复

1,401 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if the PE code was generated, try to check paths setting in project properties.

Also there should be FreeRTOS demo example within S32 Design Studio so you can try t refer to it.

BR, Petr