Error Related HSM HSM ENable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error Related HSM HSM ENable

3,439 Views
jiteshkamboj
Contributor I

I getting below error while wolfssl init. Please support, How it can be solved

jjj.png

 

0 Kudos
Reply
5 Replies

3,432 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Did you enable HSM module in DCF records?

Which HSM FW are you using?

Could you share exact package part number printed on device with me?

Best regards,

Peter

 

0 Kudos
Reply

3,419 Views
jiteshkamboj
Contributor I

HSM FW i am not aware.I did not flashed.

Is there any alternative way without using HSM FW, wolfssl can work?

0 Kudos
Reply

3,421 Views
jiteshkamboj
Contributor I

Hi Peter,

Device is mpc5748g board, Chip is SPC5748ghmku6.

0 Kudos
Reply

3,409 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Ok, so your device has HSM module, but it does not have HSM FW from NXP factory.

I assume you want to write your own HSM FW, once you finished writing HSM FW according to SHE specification you will be able to run the HSM functions.

Best regards,

Peter

0 Kudos
Reply

3,037 Views
IsaacAf
Contributor I

Hi Peter,

We want to enable HSM for MPC5746C/MPC5748G in order to perform the following:
1-Generate TRNG (HSM_DRV_InitRNG then HSM_DRV_GenerateRND then HSM_DRV_GenerateTRND)
2-Generate MAC and Verify MAC (HSM_DRV_GenerateMAC, HSM_DRV_VerifyMAC)

Please send us the DCF/Utest flash project example/Hex file in order to enable the HSM on MPC5748G/MPC5746C (spc5748ghmku6)
such that we can use HSM component "Command processor" as per your manual?

0 Kudos
Reply