Encryption mechanism

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Encryption mechanism

1,566件の閲覧回数
PENGHAN
Contributor II

 

 Hello,The chip that  I use is MPC5566. For this chip, how to set the encryption mechanism, prevent piracy from accessing the flash from the JTAG debug interface, read the software code? I Query manual does not find related encryption methods.Thank you very much.

  Respectly

0 件の賞賛
返信
1 返信

1,560件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

 

There’s no encryption on this device, there’s only censhorship feature which prevents unauthorized access via JTAG.

 

You can take a look at this application note:

https://www.nxp.com/docs/en/application-note/AN3787.pdf

https://www.nxp.com/docs/en/application-note-software/AN3787SW.zip

 

And then at this SW example:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5644A-Censorship-CW210/ta-p/1105016

It was written for MPC5644A but it’s pretty much the same for MPC5566 in terms of censhorship.

 

Regards,

Lukas

0 件の賞賛
返信