Does MPC5744B support overlay SRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does MPC5744B support overlay SRAM

828 次查看
3150100789
Contributor I

Now I have built a project based on MPC5744B, want to realize the calibration function, and then found that MPC574XX supports OverlayRAM function. After consulting the data sheet, it was found that the Flash memory base address it indicated was reserved on the chip. The specific address is as follows.

The following table shows the system memory map.

0x01780000---0x3FFFFFFF 1000 MB Reserved

On the microcontroller, the only overlay RAM target available is system RAM array0 (0x40000000 – 0x4003FFFF). There are  no restrictions within that range.

PFlash calibration remap to RAM

Flash Arrays 0x0{8,9,A}--_---- P0, P1
System RAM 0x40{0,1}-_---- P0, P1

So I want to ask if mpc5744b supports overlayram function,

thanks.

0 项奖励
回复
0 回复数