Developement environment SPC5607BF1MLU6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Developement environment SPC5607BF1MLU6

1,801件の閲覧回数
stefanschiebel
Contributor II

Hello,

I have two questions for programming an processor (SPC5607BF1MLU6):

-Can you recommend an developement environment (with an included compiler and linker) for these processor (spc5607BF1MLU6)?

-If I order the evaluation board, is it possible, to get one or two sample processors for testing?


Thank you in advance for your reply.

0 件の賞賛
返信
2 返答(返信)

1,679件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

1) I can recommend you S32 Design Studio, which is free for use.

S32 Design Studio IDE|NXP 

2) I am not sure, but I think the answer is no. You must order microcontrollers separately.

Regards,

Martin

0 件の賞賛
返信

1,679件の閲覧回数
stefanschiebel
Contributor II

Hello,

can somebody help me with that topic?

Thanks

Stefan Schiebel

Porsche Engineering Services GmbH

0 件の賞賛
返信