Picture1 show the relationship which PIT you should use when configure the DMA channel in periodic triggering mode
if i choose the DMA 16 channel , and choose the DMAMUX_1 source 3 , then which PIT channel i should configure as a periodic trigger?
DMAMUX_1.CHCFG[0].R = 0xC3;// enable periodic triggering mode ,i think PIT channel 0 or 2?
Hello,
could you please specify microcontroller you use? I need to check reference manual to tell you correct answer.
Regards,
Martin
Hello Colin,
if you use DMA_MUX in trigger mode, please ignore table 7-18 and 7-19 and see only table 7-17.
As soon as you have configured DMA_MUX in trigger mode, you can select source 0-3. If you select source 0, PIT channel 0 is used to trigger DMA channel and so on.
So, in your case, if you choose source 3, from my point of view PIT channel 3 will be used.
Regards,
Martin
1. perhaps your undersatanding of the PIT channel is not right,
cos there is no 0 source ,DMAMUX source slot count from 1 from the table 7-19
0 means DMAMUX channel trigger, corresponding PIT channel 0
e.g DMAMUX_1.CHCFG[0].R = 0xC3 this is 0 channel ,should be triggered by PIT 0 ,in desipte of which source you choose.
but the question is it is still useless when i finished to configure the PIT channel 0 , so im confused?
2. i wonder if it just transmit Data just once if the DMA is not in triggered mode(normal) ,or is there any ways to trigger the DMA multiple times if i dont use the trigger mode ,or just one way to realize the goal by putting the DMA in triggered mode ?
3. anyone ever use the multple transmit DMA function, can you give me some advices?
Hello,
I am sorry for my previous answer. It seems that things are little bit different.
For triggering, only DMA channels 0,1,2 and 3 can be used. So, you can use only DMA_MUX_0 CHCFG0 - CHCFG3. Source must be set to 24 - 29.
DMA channel 0 is connected with PIT channel 0, DMA channel 1 is connected to PIT channel 1 and so on.
I can see my colleague sent you answer in the thread below:
https://community.nxp.com/thread/504935
Regards,
Martin
can i ask you another question, if there is any chance , SPI TX buffer is full ,but not be transfered to SPI shift register ? im confused, i think ionly if TX buffer has a data, it can be transfered to SPI shift register automatically.