DEVKIT-MPC5748G CAN1 configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEVKIT-MPC5748G CAN1 configuration

3,205 Views
yuriy_serdyuk
Contributor III

Hi i have problems with CAN1 configuration (CAN0 works fine).

I have this code with PC10 and PC11 pins are connected to PCAN-USB

void peri_clock_gating (void) {  /* Configure gating/enabling peripheral(CAN) clocks */
 MC_ME.RUN_PC[0].R = 0x00000000;   /* gate off clock for all RUN modes */
 MC_ME.RUN_PC[1].R = 0x000000FE;   /* config. peri clock for all RUN modes */

 MC_ME.PCTL[70].B.RUN_CFG = 0x1;   /* FlexCAN 0: select peri. cfg. RUN_PC[1] */
 MC_ME.PCTL[71].B.RUN_CFG = 0x1;   /* FlexCAN 1: select peri. cfg. RUN_PC[1] */
}


void readCanBus1(unsigned int *id, unsigned char *buf,unsigned int len,unsigned int *outLen)
{
 uint8_t j;
 uint32_t __attribute__ ((unused)) dummy;

 while (CAN_1.IFLAG1.B.BUF4TO1I != 8) {};
 *id     = CAN_1.MB[4].ID.B.ID_STD;
 *outLen = CAN_1.MB[4].CS.B.DLC;
 if (*outLen>len)
 {
  *outLen=len;
 }

 for (j=0; j<(*outLen); j++) {
  buf[j] = CAN_1.MB[4].DATA.B[j];
 }

 dummy = CAN_1.TIMER.R;
 CAN_1.IFLAG1.R = 0x00000010;
}

void writeCanBus1(unsigned int id, unsigned char *buf,unsigned int len)
{
 uint8_t i;

 CAN_1.MB[0].CS.B.IDE = 0;
 CAN_1.MB[0].ID.B.ID_STD = id;
 CAN_1.MB[0].CS.B.RTR = 0;
 CAN_1.MB[0].CS.B.DLC = len;
 for (i=0; i<len; i++) {
  CAN_1.MB[0].DATA.B[i] = buf[i];
 }
 CAN_1.MB[0].CS.B.SRR = 1;
 CAN_1.MB[0].CS.B.CODE =0xC;
}

void initCanBus1()
{
 int i;
 CAN_1.MCR.B.MDIS = 1;
 CAN_1.CTRL1.B.CLKSRC=0;
 CAN_1.MCR.B.MDIS = 0;
 while (!CAN_1.MCR.B.FRZACK) {}
 CAN_1.CTRL1.R = 0x04DB0086;
 for (i=0; i<96; i++) {
  CAN_1.MB[i].CS.B.CODE = 0;
 }

 //TX
 CAN_1.MB[0].CS.B.CODE = 8;

 //RX
 CAN_1.MB[4].CS.B.IDE = 0;
 CAN_1.MB[4].ID.B.ID_STD = 0x666;
 CAN_1.MB[4].CS.B.CODE = 4;
 CAN_1.RXMGMASK.R = 0;//0x1FFFFFFF;

 SIUL2.MSCR[42].B.SSS = 1;     /* Pad PC10: Source signal is CAN1_TX  */
 SIUL2.MSCR[42].B.OBE = 1;     /* Pad PC10: Output Buffer Enable */
 SIUL2.MSCR[42].B.SRC = 3;     /* Pad PC10: Maximum slew rate */
 SIUL2.MSCR[43].B.IBE = 1;     /* Pad PC11: Enable pad for input - CAN1_RX */
 SIUL2.IMCR[701-512].B.SSS = 3;    /* CAN1_RX: connected to pad PC11 */

 CAN_1.MCR.R = 0x0000003F;
 while (CAN_1.MCR.B.FRZACK & CAN_1.MCR.B.NOTRDY) {}
}
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Also i try send data between CAN0 and CAN1, it doesn't work. I suppose i have some problem with configuration CAN1

Could you help me?

I know CAN1 doesn't have termination resistor. I tried connected CAN0, CAN1 and PCAN-USB parallels 

Thank you

Tags (2)
4 Replies

3,016 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm just wondering how did you connected CAN 1? Did you use external CAN transceiver connected by wires? There's CAN transceiver only for CAN 0 on this board.

Regards,

Lukas

0 Kudos
Reply

3,016 Views
yuriy_serdyuk
Contributor III

Hi Lukas, 

What does this mean. "There's CAN transceiver only for CAN 0 on this board."

According datasheet eight FlexCAN.

I have connected PB0 - PC10 - CAN-H PCAN-USB and PB1 - PC11 - CAN-L PCAN-USB

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

0 Kudos
Reply

3,016 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, there are 8 CAN modules. But one thing is CAN module, second thing is CAN transceiver defined by ISO 11898-2.

First link and picture I found on the web:

https://can-newsletter.org/assets/files/ttmedia/raw/778ff25c6a48bbd0d67b4eee94ea11ea.pdf 

pastedImage_2.png

This is what you need. Only a few MCUs have CAN transceiver implemented directly on the chip (like some of our 16bit S12 devices).

There's TJA1044GT on CAN 0 as you can see in the schematic.

TJA1044 | High-speed CAN transceiver with Standby mode | NXP 

PCAN-USB also includes high speed transceiver. It's not possible to connect CAN signals without the transceiver.

Regards,

Lukas

3,016 Views
yuriy_serdyuk
Contributor III

Hi Lukas, 

I have checked schematic my board, it's surprise for me. 

pastedImage_1.png

Thank you for information. 

0 Kudos
Reply