CodeWarrior TAP Continually Triggers System Reset Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior TAP Continually Triggers System Reset Interrupt

966 Views
ryanbrown
Contributor I

I have a "new" CodeWarrior CWH-CTP-BASE-HE USB TAP (900-76173, Rev G) that I'm trying to use with Mobile GT 9.2 in Windows 7 with a Lite5200B development board. Using an older TAP in the same setup (same probe tip, same cable, same dev board), I have no issues. Using this TAP, the debugger downloads my application with no problems, but continually enters/breaks at b __reset (0x0100 System Reset) in vectors.asm. I get the same results when using as an ethernet TAP instead of a USB TAP. I have already followed the instructions in AN4338 multiple times and am still seeing the same issues. I have also installed Codewarrior 8.8 with the 8.8.6 patch. Any help would greatly appreciated.

Tags (2)
0 Kudos
Reply
0 Replies