Cannot pull up pin C0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot pull up pin C0

894 Views
Ellison
Contributor I

        I want to use the C0 pin as the GPIO input function and configure the pull-up input mode, but the value of the pull-up BIT in the register cannot be set to 1, and the PULL function cannot be used. Is this pin only used as the ANALOG input of ADC?Can you help me? Thanks!(This image is from MPC5744PRM)微信截图_20210731091818.png

0 Kudos
Reply
0 Replies