Can not Debbuger MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not Debbuger MPC5748G

982 Views
zhaow
Contributor I

Can not Debbuger MPC5748G

Debugger Console windows:

GNU gdb (GDB build.sh rev=gceb1328 s=F494 -i /opt/freescale ELe200 -V release_gceb1328_build_Fed_ELe200_ML3 (BLD = 1607)) 7.8.2
Copyright (C) 2014 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.  Type "show copying"
and "show warranty" for details.
This GDB was configured as "--host=i686-w64-mingw32 --target=powerpc-eabivle".
Type "show configuration" for configuration details.
For bug reporting instructions, please see:
<http://www.gnu.org/software/gdb/bugs/>.
Find the GDB manual and other documentation resources online at:
<http://www.gnu.org/software/gdb/documentation/>.
For help, type "help".
Type "apropos word" to search for commands related to "word".
monitor preserve1 0
monitor preserve2 0
load D:\\A_top_S\\WorkSpace\\Pro_Space_2.1\\p456\\p456_Z4_0/../p456_Z4_1/Debug/p456_Z4_1.elf
Loading section .startup, size 0x1ee lma 0x11d0000
Loading section .core_exceptions_table, size 0xf4 lma 0x11d1000
Loading section .intc_vector_table, size 0xbc8 lma 0x11d2000
Loading section .text, size 0x3b0 lma 0x11d2bd0
Loading section .ctors, size 0x8 lma 0x11d2f80
Loading section .dtors, size 0x8 lma 0x11d2f88
Loading section .eh_frame, size 0x8 lma 0x11d2f90
Loading section .data, size 0x20 lma 0x11d2f98
Start address 0x11d0000, load size 4754
Transfer rate: 422 KB/sec, 475 bytes/write.
load D:\\A_top_S\\WorkSpace\\Pro_Space_2.1\\p456\\p456_Z4_0/../p456_Z2_2/Debug/p456_Z2_2.elf
Loading section .startup, size 0x1ee lma 0x13a0000
Loading section .core_exceptions_table, size 0xf4 lma 0x13a1000
Loading section .intc_vector_table, size 0xbc8 lma 0x13a2000
Loading section .text, size 0x3a0 lma 0x13a2bd0
Loading section .ctors, size 0x8 lma 0x13a2f70
Loading section .dtors, size 0x8 lma 0x13a2f78
Loading section .eh_frame, size 0x8 lma 0x13a2f80
Loading section .data, size 0x20 lma 0x13a2f88
Start address 0x13a0000, load size 4738
Transfer rate: 308 KB/sec, 473 bytes/write.
load D:\\A_top_S\\WorkSpace\\Pro_Space_2.1\\p456\\p456_Z4_0\\Debug\\p456_Z4_0.elf
Loading section .rchw, size 0x4 lma 0xfa0000
Loading section .cpu2_reset_vector, size 0x4 lma 0xfa0004
Loading section .cpu0_reset_vector, size 0x4 lma 0xfa0010
Loading section .cpu1_reset_vector, size 0x4 lma 0xfa0014
Loading section .startup, size 0x1f2 lma 0x1000000
Loading section .core_exceptions_table, size 0xf4 lma 0x1001000
Loading section .intc_vector_table, size 0xbc8 lma 0x1002000
Loading section .text, size 0x400 lma 0x1002bd0
Loading section .ctors, size 0x8 lma 0x1002fd0
Loading section .dtors, size 0x8 lma 0x1002fd8
Loading section .eh_frame, size 0x8 lma 0x1002fe0
Loading section .data, size 0x20 lma 0x1002fe8
Start address 0x1000000, load size 4854
Transfer rate: 263 KB/sec, 346 bytes/write.
monitor endmultiload
Ignoring packet error, continuing...
Ignoring packet error, continuing...
Ignoring packet error, continuing...

0 Kudos
Reply
0 Replies