Can I get simple CAN driver code for MPC5668G?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I get simple CAN driver code for MPC5668G?

2,196 Views
sukruthrameshba
Contributor III

I am using MPC5668G microcontroller. And I need to flash simple CAN driver code with the functionality to send and receive the frames. Can anyone attach the same?

 

Thanks,

Sukruth.

Labels (1)
0 Kudos
Reply
3 Replies

1,979 Views
sukruthrameshba
Contributor III

Hello Mr. Petr,

Thanks for your support on CAN Driver code.

I modified the sample code you sent for MPC5668G.

Its working fine for my requirements.

Thank you.

Regards,

Sukruth

0 Kudos
Reply

1,979 Views
sukruthrameshba
Contributor III

Still i am getting a stuff bit error. Please view the attached snap for the error i am getting.

Will the same code work for MPC5668g?

0 Kudos
Reply

1,979 Views
PetrS
NXP TechSupport
NXP TechSupport

See https://community.nxp.com/message/667805#comment-667805, I tested it on the EVB and it is running well.

BR, Petr

0 Kudos
Reply