CANBootLoader application in mpc5606b

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CANBootLoader application in mpc5606b

1,664 次查看
xy387
Contributor I

I want to tell the linker to build for the starting address of the intended AppSlot,so I made some change in my link file ,but it does not work ,and my program dead. by the way, The MCU I used is MPC5606B, The IDE is CW10.6,  I do not know where is my problem. Anyone could tell me where is my fault. I appreciate all your help,Thank you very much.

 

This is where my change

resetvector:                  org = 0x00010000,   len = 0x00000008

init:                               org = 0x00010008,   len = 0x00000FF0

exception_handlers:    org = 0x00011000,   len = 0x00002000

internal_flash:              org = 0x00013000,   len = 0x000ED000

 

This is my original link file

/* Internal FLASH linker command file for MPC5606B                          */

/*                                                                          */

/*                 1MB Flash, 80KB SRAM                                     */

/*                                                                          */

/* Intended to be used for the stationary example project.                  */

/*                                                                          */

/* VERSION: 1.1                                                             */

/*                                                                          */

 

 

MEMORY

{

    /*FLASH: 0x00000000 - 0x0000FFFFF*/

 

 

    /* Fixed location required for RCHW and program entry point. */

    resetvector:           org = 0x00000000,   len = 0x00000008

 

 

    /* Contains initializations from __ppc_eabi_init.c,

     MPC56xx_HWInit.c, MPC56xx_init_*.c and the entry point (__startup).

     */

    init:                  org = 0x00000008,   len = 0x00000FF0

 

 

    /* Contains interrupt branch tables for both core and INTC module

     and the ISR handlers code. Note, since the vector base address field

     of IVPR is defined within the range [0:19] the table must be loaded

     at an address aligned to 4K boundary.

     */

    exception_handlers:    org = 0x00001000,   len = 0x00002000

 

 

    /* Space allocated for user code and device initialization.

    ROM Image address should be set with the start address of this

    segment in order to instruct the runtime to initialize the

    static variables. All the section above are ignored for this action.

    Please see -romaddr linker option.*/

    internal_flash:        org = 0x00003000,   len = 0x000FD000

 

    /* SRAM: 0x40000000 - 0x40013FFF */

    internal_ram:          org = 0x40000000,   len = 0x00012000 /* 72K */

    heap  :                org = 0x40012000,   len = 0x00001000 /* 4K */

    stack :                org = 0x40013000,   len = 0x00001000 /* 4K */

}

 

 

/* This will ensure the rchw and reset vector are not stripped by the linker */

FORCEACTIVE { "bam_rchw" "bam_resetvector" }

 

 

SECTIONS

{

    .__bam_bootarea LOAD (ADDR(resetvector)): {} > resetvector

 

    GROUP : {

    /* Section used for initialization code: __ppc_eabi_init.c,

     MPC56xx_HWInit.c, MPC56xx_init_*.c and the entry point (__startup).

     */

      .init LOAD(ADDR(init)) : {}

      .init_vle (VLECODE) LOAD(_e_init) : {

        *(.init)

        *(.init_vle)

      }

    } > init

  

    GROUP : {

    /* Fixed length of 0x800 is required for core interrupt branch table.

    Core IVOR branch table entries must be aligned to 16 bytes.

    */

    .ivor_branch_table (VLECODE) LOAD(ADDR(exception_handlers)) ALIGN (0x10) : {}

 

    /* Note if intc_hw_branch_table is used it MUST be loaded at the IVPR + 2KB (0x800).

     For this device the intc_hw_branch_table should contain entries aligned to 4 bytes.

     */

    .intc_hw_branch_table (VLECODE) LOAD(_e_ivor_branch_table) ALIGN(0x800) : {}

 

    /* ISR handlers code.*/

    .__exception_handlers  (VLECODE) LOAD(_e_intc_hw_branch_table) : {}

    } > exception_handlers

 

 

    GROUP : {

      .text : {}

      .text_vle (VLECODE) ALIGN(0x08): {

         *(.text)

         *(.text_vle)

       }

       .rodata (CONST) : {

         *(.rdata)

         *(.rodata)

       }

    

       .ctors : {}

       .dtors : {}

       extab : {}

       extabindex : {}

    } > internal_flash

 

 

    GROUP : {

        /* The INTC module for this device contains up to 221 IRQs.*/

       .__uninitialized_intc_handlertable ALIGN(2048) : {}

       .data   : {}

       .sdata  : {}

       .sbss   : {}

       .sdata2 : {}

       .sbss2  : {}

       .bss    : {}

    } > internal_ram

}

 

 

/* Freescale CodeWarrior compiler address designations */

 

 

_stack_addr = ADDR(stack)+SIZEOF(stack);

_stack_end  = ADDR(stack);

_heap_addr  = ADDR(heap);

_heap_end   = ADDR(heap)+SIZEOF(heap);

 

 

 

 

/* Exceptions Handlers Location (used in Exceptions.c IVPR initialization)*/

EXCEPTION_HANDLERS = ADDR(exception_handlers);

 

 

/* L2 SRAM Location (used for L2 SRAM initialization) */

L2SRAM_LOCATION = ADDR(internal_ram);

 

 

/* How many writes with stmw, 128 bytes each, are needed to cover

   the whole L2SRAM (used for L2 SRAM initialization) */

L2SRAM_CNT = 0x14000 / 128;

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,210 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at:

https://community.freescale.com/message/427962#comment-427962

I described how to create projects for application/bootloader in chapter 2.

Lukas

0 项奖励
回复