CAN with internal IRC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN with internal IRC

1,520件の閲覧回数
keerthidhanapal
Contributor I

I have configured a CAN with peripheral clock. And the system is running with 16MHZ IRC. 

 

The CAN communication is not seems to be consistent. Most of the time it works but sometime its struct with error ISR of CAN.

 

Can you give your view on this?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,394件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately you did not specify the device, so just generally.

There are several requirements coming from the FlexCAN module, in summary…

- A valid CAN bit timing must be programmed, as indicated in RM.

- The peripheral clock frequency can not be smaller than the selected CPI clock frequency.

- There must be a minimum ratio between the peripheral clock frequency and the CAN bit rate, as specified in “Arbitration and Matching Timing” chapter of the RM.

BR, Petr

0 件の賞賛
返信