Add new section to RAM from linker file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Add new section to RAM from linker file

1,032 Views
elb1
Contributor III

Hello, i want to save some variables directly to a known RAM section.
So to test that 
i have opened hello_world example project for MPC5746C, but it doesn't work:

This is the detail of what i added to hello_world example project:

in the main file:

#define _TEST_ __attribute__ ((section (".testsection")))

uint8_t test1 _TEST_ = 1;

uint8_t test2 _TEST_ = 2;

uint8_t test3 _TEST_ = 3;

 

int main(void)

{

.......

}

 

In the linker file:

1. if i add this after the definition of .rodata section like this :

  .testsection: ALIGN(0x10)

  {

    KEEP(*(.testsection))

    . = ALIGN(0x10);

  } > m_data AT> m_text

 

the variable test1, test2, and test3 will go to the address 0x40000000 (i can see it in the map file) but when i debug and i browse that address i will find 00000000 instead of 01020300.

 

2. if i add this between the definition of .sdata and .data like this :

 

__TEST_ROM = __DATA_END;

.testsection : AT (__TEST_ROM)

{

. = ALIGN(0x10);

__TEST_RAM = .;

__test_start__ = .;

KEEP(*(.testsection))

__test_end__ = .;

} > m_data

__TEST_END = __TEST_ROM + (__test_end__ - __test_start__);

 

I will get this error :

section .sdata LMA [01003337,01003337] overlaps section .caldata LMA [01003334,01003342]

 

 

Thank you in advance,
Looking forward for your response

0 Kudos
Reply
1 Reply

961 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share the full linker script file? 

0 Kudos
Reply