About the S32DS installation DIAB software compilation error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the S32DS installation DIAB software compilation error

3,473件の閲覧回数
lubo_NEW
Contributor III

According to the documentation to NXP has installed the DIAB compiler plug-in, after the installation to create a simple file but always prompt error
The following
"../Sources/main.c", fatal error (etoa:1635): License error: Unknown LMAPI error

0 件の賞賛
返信
3 返答(返信)

3,451件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @lubo_NEW,

Are you able to invoke the Diab compiler from the command line? Have you confirmed your license for Diab is valid?

Best Regards,

Mike

0 件の賞賛
返信

3,473件の閲覧回数
lubo_NEW
Contributor III

1111.png

The DIAB compiler license is not enabled

0 件の賞賛
返信

3,014件の閲覧回数
jacst
Contributor II

Hello, have you solved this problem? I also encountered it, and found that deleting the debug folder, closing the project and opening it can compile normally

0 件の賞賛
返信