AUTOSAR OS for MPC5634

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AUTOSAR OS for MPC5634

1,298件の閲覧回数
Vasily_Wu
Contributor III

Hello all,

I have downloaded the source code of AUTOSAR OS for MPC5634, there I have some questions:

1) I don't have any Lauterbach for debugging. Could I port the source code into Codewarrior, then using PE to debug?

2) I am using EB Tresos for generating the CFG code. Does this AUTOSAR OS independent with AUTOSAR MCAL?

3) Any use manual for porting AUTOSAR OS.

Thank you!

0 件の賞賛
返信
1 返信

1,288件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello @Vasily_Wu,

1) You should build the application first via make GNU. Then you can take the elf file to load into the MCU using PE and S32DS.

2) Yes, AUTOSAR OS is independent.

3) Unfortunately, that document is not available.

Best Regards,

Nam

0 件の賞賛
返信