AUTOSAR OS for MPC5634

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AUTOSAR OS for MPC5634

1,296 Views
Vasily_Wu
Contributor III

Hello all,

I have downloaded the source code of AUTOSAR OS for MPC5634, there I have some questions:

1) I don't have any Lauterbach for debugging. Could I port the source code into Codewarrior, then using PE to debug?

2) I am using EB Tresos for generating the CFG code. Does this AUTOSAR OS independent with AUTOSAR MCAL?

3) Any use manual for porting AUTOSAR OS.

Thank you!

0 Kudos
Reply
1 Reply

1,286 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @Vasily_Wu,

1) You should build the application first via make GNU. Then you can take the elf file to load into the MCU using PE and S32DS.

2) Yes, AUTOSAR OS is independent.

3) Unfortunately, that document is not available.

Best Regards,

Nam

0 Kudos
Reply