5606S problem when return from standby

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

5606S problem when return from standby

1,764 Views
miquel_soler
Contributor I

Hi everybody.

 

I have some problems in standby mode exit with MPC5606S CPU

 

The source code is based on "Low power modes" from freescale examples for MPC5606S.

 

The purpose of the source code is to wait from 2 wakeup sources to exit from standby mode

#define IN_IGNITION   19    // IN_IGNITION   -> PB3  GPIO[19]  uC_PIN 110

#define IN_HNBR_L_SW1 75    // IN_HNBR_L_SW1 -> PF5  GPIO[75]  uC_PIN 117

 

In run mode, the code checks what is the wake-up source and flashes some LED. If the wakeup GPI line is low, come back to standby mode.

Additionally in run mode the main clock is send out by PH[4] GPIO to check the frequency.

 

The system seems to be working correctly but there are some problems that I can't fix.

Starting from power supply OFF to ON, the CPU need 3 or 4 wake-up event to start to flash the LED.

Checking the power consumption, when the wake-up GPI line is active, the CPU current consumption increase and flash some LED very fast.

Checking the clock output line. I see that:

1) In the cases that the CPU works (LED flashing) the clock is 64MHz and the system works fine

2) In the cases that the CPU not wake-up OK (very fast LED flash), the clock start to oscillate for 500ns and then stabilize the frequency at 64MHz for 3us, after these 3us, the oscillation stop.

 

I do the same test using different clocks source (XTAL, PLL and internal 16MHz rc oscillator) and the results are the same.

 

I thing I'm doing something wrong but I can't fine the mistake.

Can somebody help me to fine the problem.

 

Thanks

 

Miquel Soler i Mir

Original Attachment has been moved to: main.c.zip

Labels (1)
0 Kudos
Reply
2 Replies

1,584 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure all wake up flags are really cleared before going to low power mode.

Also you should set pull-ups to all wake up sources, so use WKUP.WIPUER.R = 0x001FFFFF;

Regards

Petr

0 Kudos
Reply

1,584 Views
miquel_soler
Contributor I

Hi,

The two wake-up inputs are pulled down externally.

In line 195 before to enter into standby mode, the wake up flag are cleaned.

0 Kudos
Reply