Example MPC5777C-eTPU_GPIO_test GHS714

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5777C-eTPU_GPIO_test GHS714

Example MPC5777C-eTPU_GPIO_test GHS714

********************************************************************************
* Detailed Description:
* A simple example configures eTPU engine B channels 0/1 for GPO/GPI. It is
* needed to connect these pins by wire. Output wave is generated by eTPU GPIO
* output function and inputs are read by fs_etpu_gpio_input_immed function
* latching just current pin state. Pin history is displayed in ISR.
*
* Note: It is needed to configure IGF module, otherwise inputs does not pass
* to eTPU module.
*
* ------------------------------------------------------------------------------
* Test HW:         MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C
* MCU:             PPC5777CMM03 2N45H CTZZS1521A
* Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz
* Debugger:        Lauterbach Trace32
* Target:          internal_FLASH
* Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A
* EVB connection:  ETPUB0 (PortR P25-1) --> ETPUB1 (PortR P25-0) by wire
*
********************************************************************************

タグ(2)
添付
コメント

Hello David,

As I know, the input of ETPU channel can be connected from the SDADC valid data flag output or the external pad, we use the SIU_SDETPUA, SIU_SDETPUB, SIU_SDETPUC to choose the connection .You can see the below image:

SDADC_ETPU.png

- I use ETPUA channel 9:

      + In the case 1, ETPUA_9 is connected to the external pad, the pinstate returned by fs_etpu_gpio_pin_history is correct as expected.

      + In the case 2,  ETPUA_9 is connected to the SDADC1 data valid flag output, the pinstate returned by fs_etpu_gpio_pin_history always be 0 even though the SDADC1 Conversion Data Valid Event is enabled(CDVEE bit of SDADC_RSER is 1) and Converted Data Valid Flag is 1(CDVF bit of SDADC_SFR is 1). This is wrong. I don't know why.

- The difference between these 2 cases is just SIU_SDETPUA configuraion.

Do you know why?

Regards,

Tam

Sorry, the ETPU channel is ETPUA_15

I tried with 2 cases:

- The ETPUA_15 channel with SDADC2

- The ETPUA_9 channel with SDADC1.

The pinstate always be 0.

Hi, please create new thread here on the community space or new case according to following procedure:
https://community.nxp.com/docs/DOC-329745

評価なし
バージョン履歴
最終更新日:
‎10-17-2017 11:16 PM
更新者: