Example MPC5777C TSENS Temperature calculation GHS614

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5777C TSENS Temperature calculation GHS614

Example MPC5777C TSENS Temperature calculation GHS614

********************************************************************************

* Detailed Description:

*

* Example shows MCU's temperature measurement with the help of TSENS.

* Calibartion constants for TSENS0/TSENS1 are read from Test flash and

* eQADC is set to measure Vbg and TSENS outputs. eQADC calibration is also done.

* Calculated internal temperature can be displayed on the Terminal.

*

* See results on PC terminal (19200, 8N1, None). You should see following text

* (with different values for sure)

*

*    TSENS0/TSENS1 temperature measurement

*     press any key to continue...

*

*    Calibration constants read from TSENS registers

*

*    TSENS0                           TSENS1

*

*    TSCA_0 = 207                     TSCA_1 = 148

*    TSCB_0 = 7                       TSCB_1 = 19

*

*    T = (232 + TSCA * 2^-6) * TSENS_CODE_T / VBG_CODE_T - (273 + TSCB * 2^-4) [degC]

*

*    VBG_CODE_T   =  997

*    TSENS0_CODE_T = 1325             TSENS1_CODE_T = 1332

*

*    TSENS0 temp = 39.19 degC         TSENS1 temp = 38.86 degC

*

* ------------------------------------------------------------------------------

* Test HW:         MPC5777C-512DS Rev.A + MPC57xx MOTHER BOARD Rev.C

* MCU:             PPC5777CMM03 2N45H CTZZS1521A

* Fsys:            PLL1 = core_clk = 264MHz, PLL0 = 192MHz

* Debugger:        Lauterbach Trace32

* Target:          internal_FLASH

* Terminal:        19200-8-no parity-1 stop bit-no flow control on eSCI_A

*                  use USB connector (J21) on minimodule

* EVB connection:  ETPUA30 (PortP P23-15) --> USER_LED_1 (P7-1)

*                  ETPUA31 (PortP P23-14) --> USER_LED_2 (P7-2)

*

********************************************************************************

ラベル(1)
添付
コメント

"I measured it in the same way, but the ADC voltage for TempSense 1, TempSense 2, and the bandgap voltage is continuously varying. Is this expected? Because of this, the temperature values keep changing.

Here are the calibration values I retrieved from flash memory:
- TempSensor_0_Calibration_A: 237
- TempSensor_0_Calibration_B: 54
- TempSensor_1_Calibration_A: 127
- TempSensor_1_Calibration_B: 1

And the following are the current measured values:
- VBG_CODE_T: 1065
- TSENS_CODE_T_1: 1393
- TSENS_CODE_T_2: 1229

These values fluctuate, and sometimes they even go negative. Are these variations normal?"

評価なし
バージョン履歴
最終更新日:
‎02-25-2016 07:19 AM
更新者: