Example MPC5646C eMIOS frequency measurement CW210

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5646C eMIOS frequency measurement CW210

Example MPC5646C eMIOS frequency measurement CW210

********************************************************************************
* Detailed Description:
*
* This example shows possible implementation of frequency and duty cycle

* measurement with the help of eMIOS module.
* Two eMIOS channels are used and set to IPWM and IPM modes. The first channel
* measures the positive pulse width and the second channel measures the period.
*
* EVB connection:
* PJ7.5 to PJ7.6 ... connect external pulse signal to this
*
* See result on PC terminal (9600, 8N1)
* ------------------------------------------------------------------------------
* Test HW:  XPC56xxMB2 + XPC564xB/C, SPC5646C 0N32E silicon
* Target :  internal_FLASH, RAM
* Fsys:     120 MHz PLL0
* Debugger: Lauterbach Trace32. script for internal_FALSH run_from_flash.cmm
*                               script for RAM: run_from_ram_vle.cmm
*
********************************************************************************

 

183024_183024.pngpastedImage_2.png

 

BR, Petr

Labels (1)
Attachments
Comments

Why can printf work? How can I use this function via CAN?

my email: [email protected]

Link to source file no longer works.  Where did you put the code?

link is restored. BR, Petr

No ratings
Version history
Last update:
‎05-03-2017 04:22 AM
Updated by: