Example MPC5607B CAN sampler and STOP mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5607B CAN sampler and STOP mode

Example MPC5607B CAN sampler and STOP mode

********************************************************************************

* Detailed Description:

* This example shows how to configure Wake up unit and CAN sampler.

* Once the device is woken up from STOP mode by falling edge on CAN0RX pin,

* the CAN sampler starts to sample this pin in given period.

* FlexCAN module is not initialized and used in this example because the CAN

* sampler is independent of FlexCAN.

* ------------------------------------------------------------------------------

* Test HW:  XPC56xxMB2 + XPC560B 176LQFP, PPC5607B

* Target :  internal_FLASH, RAM

* Fsys:     64 MHz PLL

*

********************************************************************************

标签 (1)
附件
无评分
版本历史
最后更新:
‎03-24-2014 04:33 AM
更新人: