Example MPC5606S-STOP_mode_implementation CW210

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5606S-STOP_mode_implementation CW210

Example MPC5606S-STOP_mode_implementation CW210

Detailed Description:
* This example shows, how to configure Mode entry module and enable required
* peripherals only. RTC module is configured to create interrupt every 50ms.
* Microcontroller is in in STOP mode most of the time and it is waken-up using RTC
* interrupt.
*
* ------------------------------------------------------------------------------
* Test HW:         XPC560S 144LQFP, XPC56XX EVB MOTHEBOARD Rev.C
* MCU:             PPC5606S 0M25V
* Terminal:        
* Fsys:            16MHz IRC
* Debugger:        Lauterbach Trace32
*                  PeMicro USB-ML-PPCNEXUS
* Target:          RAM, internal_FLASH
* EVB connection:  Default
*
********************************************************************************

附件
无评分
版本历史
最后更新:
‎04-27-2017 11:45 PM
更新人: