unable to enumerate USB device (NXP i.mx 8M PLUS)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unable to enumerate USB device (NXP i.mx 8M PLUS)

1,730件の閲覧回数
SAURAVMISHRA95
Contributor I

root@imx8mp-lpddr4-evk:~# cd /run/meida/[ 275.658219] usb 2-1: USB disconnect, device number 3
[ 275.838584] FAT-fs (sda1): unable to read boot sector to mark fs as dirty
[ 277.294801] usb usb1-port1: Cannot enable. Maybe the USB cable is bad?
[ 278.262494] usb usb1-port1: Cannot enable. Maybe the USB cable is bad?
[ 278.262711] usb usb1-port1: attempt power cycle
[ 279.306791] usb usb1-port1: Cannot enable. Maybe the USB cable is bad?
[ 280.274494] usb usb1-port1: Cannot enable. Maybe the USB cable is bad?
[ 280.274729] usb usb1-port1: unable to enumerate USB device

 

root@imx8mp-lpddr4-evk:/sys/bus/pci/drivers# ls -l /sys/bus/pci/drivers/ehci-pci
total 0
--w------- 1 root root 4096 Feb 29 18:48 bind
--w------- 1 root root 4096 Feb 29 18:48 new_id
--w------- 1 root root 4096 Feb 29 18:48 remove_id
--w------- 1 root root 4096 Feb 29 18:40 uevent
--w------- 1 root root 4096 Feb 29 18:48 unbind

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,725件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board are you using? NXP reference board?

0 件の賞賛
返信

1,717件の閲覧回数
SAURAVMISHRA95
Contributor I

i am using NXP i.MX 8M PLUS LPDDR 4-EVK BOARD

 

0 件の賞賛
返信

1,705件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

OK, got it, could you tell me which version BSP are you using and give the details steps in your side, I will try the same steps in our board and then see if problmem can be reproduced. Great thanks

0 件の賞賛
返信

1,634件の閲覧回数
SAURAVMISHRA95
Contributor I

Step1:-downloaded BSP for i.MX8M Plus EVk board https://www.nxp.com/webapp/sps/download/license.jsp?colCode=REAL-TIME_EDGE_V3.1_IMX8MP-LPDDR4-EVK&ap...

zephyr download:-https://docs.zephyrproject.org/latest/boards/nxp/imx8mp_evk/doc/index.html

configure M7 native :-imx8mp-cm7 in remoteproc0 

root@imx8mp-lpddr4-evk:~# cat /sys/class/remoteproc/remoteproc0/name
imx8mp-cm7

i am trying to run zephyr in M7 core of i.MX 8M Plus evk board.After cross compiling the zephyr file and created .elf and .bin file.

step 2:-taking these file to board ---> /lib/firmware section.

step 3:-running following these two commands:-

# echo zephyr.elf > /sys/class/remoteproc/remoteproc0/firmware

# echo start > /sys/class/remoteproc/remoteproc0/state

step4:- following error is coming in the board and execution stucked:-

root@imx8mp-lpddr4-evk:~# ls
firmware nservo_example open62541_example state work zephyr zephyr.elf
root@imx8mp-lpddr4-evk:~# echo zephyr.elf > /sys/class/remoteproc/remoteproc0/firmware
root@imx8mp-lpddr4-evk:~# echo start > /sys/class/remoteproc/remoteproc0/state
[ 90.686307] remoteproc remoteproc0: powering up imx8mp-cm7

0 件の賞賛
返信

1,532件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Thanks for your detailed steps,   @SAURAVMISHRA95 

could you please let me know which zephyr demo you are using?  I'd like to reproduce this on my side.

Please kindly note that Zephyr must explicitly enabled and configure USB support in the device tree and Kconfig.

You can check the kernel log to see whether USB is initialized correctly?

I noticed below error message,

usb usb1-port1: Cannot enable. Maybe the USB cable is bad?     


this could be a hardware issue, please double check it on your side, try to replace the USB cable?

 

Regards

Daniel

usb usb1-port1: Cannot enable. Maybe the USB cable is bad?

0 件の賞賛
返信