nboot_sb3_load_manifest issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

nboot_sb3_load_manifest issues

1,219件の閲覧回数
psmitty7373
Contributor II

When using the nboot_sb3_load_manifest API on a MCXN236, are any keys for the firmware required to be loaded into the device in the customer area or can everything be set using the nboot_sb3_load_manifest_parms_t structure?  When attempting to load a simple sb3 file with known keys, known certs, nboot_sb3_load_manifest always fails.  Even the example code from the FRDM-RW612 fails (https://github.com/nxp-mcuxpresso/mcux-sdk-examples/blob/52b428258efda7d5bd8a2ace2195ca828356743a/fr...).  What are the requirements for the nboot_sb3_load_manifest call to succeed?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

950件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

 Hi @psmitty7373 

To get more documentation regarding the NBOOT please consult the security reference manual of the MCX N236. The manual  is available under signed NDA. If you need more information about the NDA please refer to this link https://www.nxp.com/support/support/non-disclosure-agreement-faqs:NDA-FAQS

Diego

0 件の賞賛
返信