nboot_sb3_load_manifest issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nboot_sb3_load_manifest issues

1,214 Views
psmitty7373
Contributor II

When using the nboot_sb3_load_manifest API on a MCXN236, are any keys for the firmware required to be loaded into the device in the customer area or can everything be set using the nboot_sb3_load_manifest_parms_t structure?  When attempting to load a simple sb3 file with known keys, known certs, nboot_sb3_load_manifest always fails.  Even the example code from the FRDM-RW612 fails (https://github.com/nxp-mcuxpresso/mcux-sdk-examples/blob/52b428258efda7d5bd8a2ace2195ca828356743a/fr...).  What are the requirements for the nboot_sb3_load_manifest call to succeed?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

945 Views
diego_charles
NXP TechSupport
NXP TechSupport

 Hi @psmitty7373 

To get more documentation regarding the NBOOT please consult the security reference manual of the MCX N236. The manual  is available under signed NDA. If you need more information about the NDA please refer to this link https://www.nxp.com/support/support/non-disclosure-agreement-faqs:NDA-FAQS

Diego

0 Kudos
Reply