Hi,
I find file SPF31399, R6 is DNP; another file SPF47712 is same, the MT53D512M32D2DS is dual die, So, should 240-ohm resistors be placed R6?
Which vision is the latest?
MT53D512M32D2DS will EOL, we wanted to replace it to MT53E1G32D2FW, may I ask which parts of the hardware need to be modified? Or is it completely compatible without the need to modify the PCB?
Thanks! HW-Open-Source #i.MX8 mini