a replacement product for MCF51JE256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

a replacement product for MCF51JE256

309 Views
ly_12_31
Contributor I

I would like to ask for your recommendation on an MCU chip that meets the following requirements: 32-bit data bus/transfer Program memory space of 1 MByte or larger Integrated with at least one I2C bus controller Integrated with at least two SPI bus controllers At least six or more A/D analog-to-digital conversion channels Integrated with at least a 3×3 matrix keyboard controller Integrated with at least two or more timers Integrated with TOD (Time-of-Day) timer interrupts and other external interrupts Integrated with a USB interface controller That is all — thank you for your help. We hope to find a chip that can replace the functionality of the MCF51JE256, which is our current chip. If you'd like, I can also help you search for specific MCU recommendations that match these requirements.

0 Kudos
Reply
2 Replies

155 Views
ly_12_31
Contributor I
Dear Alice,
Thank you for your reply, and thank you for the alternative chip solutions your company previously recommended — they have been very helpful to our evaluation.
At present, our company is assessing the feasibility of alternative chips from multiple perspectives, and the specific solution is still under further review and confirmation. Once the plan is finalized, we will communicate with you in a timely manner and look forward to advancing the next steps of cooperation with your company.
Thank you again for your support and assistance!
 
Best regards,
Liu Ying
0 Kudos
Reply

246 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ly_12_31 

I recommend considering the MCXA or MCXN series, as they are NXP's latest mainstream MCU families and are actively promoted for new designs.

These devices can meet all of your requirements except for the dedicated 3×3 matrix keyboard controller. However, this functionality can be implemented using GPIOs in software.

 

MCX A13 A14x MCX A15x Arm Cortex-M33- Low Power and Intelligent Peripherals | NXP Semiconductors

MCX N94, N54, N53, N52 and N24 MCUs | NXP Semiconductors 

 

Thank you.

 

BR

Alice

0 Kudos
Reply