Why does the FRDM‑MCXA346 Design Files archive contain a schematic for FRDM‑MCXA166?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does the FRDM‑MCXA346 Design Files archive contain a schematic for FRDM‑MCXA166?

Jump to solution
2,113 Views
igoreq1010
Contributor I

Hello,

while reviewing the FRDM‑MCXA346 design files from the NXP download section, I noticed that the included schematic is labeled for FRDM‑MCXA166 instead of FRDM‑MCXA346.

Could you clarify:

  1. Is this intentional and are both boards sharing the same schematic?

  2. Or is this a packaging error in the archive?

  3. Are the MCXA166 and MCXA346 MCUs actually different devices, or is MCXA346 just a newer designation for MCXA166?

I would appreciate if someone from NXP could confirm whether the provided schematic is correct for FRDM‑MCXA346.

I downloaded the archive from the NXP page, and it is named "FRDM‑MCXA346‑DESIGN‑FILES.zip"

 

Thanks in advance!

— Igor

Labels (1)
0 Kudos
Reply
1 Solution
1,768 Views
Habib_MS
NXP Employee
NXP Employee

Hello @igoreq1010,

The link has been updated, and the design files for the FRDM‑MCXA346 are now available for download.
BR
Habib

View solution in original post

2 Replies
1,769 Views
Habib_MS
NXP Employee
NXP Employee

Hello @igoreq1010,

The link has been updated, and the design files for the FRDM‑MCXA346 are now available for download.
BR
Habib

2,026 Views
Habib_MS
NXP Employee
NXP Employee

Hello @igoreq1010,


Thank you for letting us know. We are working to resolve this issue. I appreciate your patience and will get back to you as soon as we update the link.

BR
Habib.

0 Kudos
Reply