Using USB on Core 1 of LPC55S6X (Zephyr OS)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using USB on Core 1 of LPC55S6X (Zephyr OS)

2,486 Views
alexfeinman
Contributor III
Spoiler
I am trying to figure out what needs to be done to assign a USB peripheral (device controller) to the CPU1 of LPC55S69 (LPCXPRESSO board)

I am building a modified cdc-acm sample project. The main core (CPU0) is flashed with a build that enabled CPU1. I have no issues running code on CPU1. I can for example handle button presses. But USB hardware does not initialize correctly. For example I see that inside USB_EhciPhyInit all writes to usbPhyBase->CTRL do not change its value from 0 (I am using Ozone debugger to look at the hardware registers).

To summarize - it looks like both USBPHY and USBHSD register ignore writes from the driver.


Things I've checked:

1. Same project works on CPU0
2. USB controllers and USB RAM are disabled in the CPU0 project I use to initialize and start CPU1
3. USB controllers and USB RAM are enabled on CPU1

Basically I hit the same SW path through the USB initialization as on  CPU0 except the peripherals seem to be dead - as if the clock was not enabled
Labels (1)
0 Kudos
Reply
4 Replies

2,456 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi  @alexfeinman 

On LPC55S69 the two M33 cores share the same peripherals, but CPU1 has no TrustZone, and by default many peripherals come up as Secure‑only.

LPCXPRESSO55S69 — Zephyr Project Documentation

Harry_Zhang_0-1770715804895.png

BR

Harry

0 Kudos
Reply

2,415 Views
alexfeinman
Contributor III

Thank you. If I understand your reply correctly, my choice is to either use non-secure build on CPU0 or to configure trust zone to allow CPU1 USB access somehow. Could you point me to any resources on how to achieve the latter in Zephyr?

0 Kudos
Reply

2,327 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @alexfeinman 

CPU1 (the second Cortex‑M33 in LPC55S69) does NOT support TrustZone at all.

You cannot "configure TrustZone to allow CPU1 USB access" in Zephyr.

May i ask what is your goal?

only USB device running on CPU1?
 
BR
Harry
0 Kudos
Reply

2,053 Views
alexfeinman
Contributor III

Apologies for late reply. Somehow notification emails ended up in junk folder.

My goal is to have the code handling the USB interface running on core 1, while core 0 is doing something unrelated. Essentially I want to use core 1 as a dedicated communication processor running multiple UART to USB bridges (4 total).

0 Kudos
Reply