Using FRDM MCXW71 as USB HID device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using FRDM MCXW71 as USB HID device

1,583 Views
enzoGrieneisen
NXP Employee
NXP Employee

I have a FRDM-MCXW71 board and I want to used it as a USB HID device. The MCXW71 cannot support USB HID but I noticed this link:
MCU-Link Debug Probe Architecture | NXP Semiconductors
where it seems like I can reflash the LPC on the FRDM board to act a USB HID device. I downloaded the package but there is no info about how to use it. Is it still possible? 

Thank you

Labels (2)
0 Kudos
Reply
1 Reply

1,534 Views
sofiaurueta
NXP Employee
NXP Employee

Hello, hope you are doing well!

 

The LPC can be configured to operate as a USB HID device. However, this would require replacing the existing MCU-LINK firmware on the LPC with a new application that implements the USB HID functionality. In addition, a communication interface (UART) must be established between the LPC and the MCXW71 device to transfer data from the MCXW71 BLE application.

 

It is important to note that replacing the MCU-LINK firmware will eliminate the onboard debugging and programming capabilities, since the LPC is currently responsible for SWD functionality, so an external debugger would be necessary in order to implement the debugging capabilites.

 

Best regards,
Ana Sofia.

0 Kudos
Reply