Unused NTC connections MC33775

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unused NTC connections MC33775

706件の閲覧回数
bg18
Contributor I

Are there any hardware considerations for unused NTC/GPIO connections on the MC33775  or MC33774 ?

I found useful information for using the mentioned chips with less than 14 cell measurements, do unused GPIO pins need to be biased with hardware or just the registers disabled in software?

ラベル(2)
0 件の賞賛
返信
1 返信

682件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi bg18

It's a good practice to either configure the GPIO pin as an input and use a pull-up or pull-down resistor to provide a defined voltage level when the input is not connected, or configure the GPIO pin as an output and set it to a known state.

0 件の賞賛
返信